This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM3481: LM3481

Part Number: LM3481

Tool/software: WEBENCH® Design Tools

We are designing boost converter with LM3481 using WEBENCH for following specifications

I/P Voltage-5V

OUTPUT-12V,1A

During hardware testing we found that no load voltage is 12V but after connecting 12 ohms resistive load,o/p voltage is 5V.As we increases output load from 12 ohms to higher value like 300 ohms output voltage increase from 5V to 12v. output voltage is not constant. PFA schematic attached.Please suggest solution for this issue.