This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/ADS4145: ADS4145 tools

Part Number: ADS4145


Tool/software: WEBENCH® Design Tools

hi,

i try to operate TIGAR_release1P4 after i installed MCR and get this error message :

My Own Exception: Fatal error loading library C:\Program Files (x86)\MATLAB\MATLAB Compiler Runtime\v79\bin\win32\mclmcr.dll Error: The application has failed to start because its side-by-side configuration is incorrect. Please see the application event log or use the command-line sxstrace.exe tool for more detail.

i have windows 10 operation system.

i regards a help to play correct this application.

thanks,

yinon