Tool/software: WEBENCH® Design Tools
Hi Team,
Our customer is simulating with LMZM33606 in WEBENCH with the following conditions:
Vout = 12V
Vin = 24V typical
Vin lowest = 13.5V (When operating from battery)
Output Current = 4A or higher
However, WEBENCH was unable to create the design due to stability issues caused by phase margin being beyond 35°-120°. Can you help us identify what is causing this?
Aside from minimum Vin being 1.1*Vout, are there any other considerations to keep in mind on these operating conditions?
Thank you very much in advance.
Kind Regards,
Jejomar