Part Number: TIDA-010038
Other Parts Discussed in Thread: PMP20199, PMP40025, PMP40467
Hi TI team,
Customer reviewed TIDA-010038. they try to design a charging system.
Battery : 48V
Charging voltage : 55V
Charging current : min 0.2A, typical : 0.4A, max : 0.5A
1. Do you have a sheet for calculating the parameter appropriate for the output voltage and current? If you don't have a parameter calculation sheet, can you tell me which point to change?
2. Can you tell me which block corresponds to the CC feedback loop?
Thanks.