Part Number: TIDA-01518
Hi,
are there any suggestions for sensors for the actual water leak?
Is there a list of manufacturers? Are any of them making a sensor cable?
Thank you!
Regards,
Alberto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01518
Hi,
are there any suggestions for sensors for the actual water leak?
Is there a list of manufacturers? Are any of them making a sensor cable?
Thank you!
Regards,
Alberto
Hi Alberto,
For the water leak sensing, the TIDA-01518 design leverages a single transistor and two prongs. Once the resistance is reduced from the presence of water between the contacts, the alarm goes off. As far as the recommended sensors, from what we have seen, most use this same method, so I am not aware of any actual "sensor" that can do the same. Let me look into this and get back to you with a definitive answer.
-Brian
Alberto,
After doing some research, I found a few company that have cable style probes for water leak detection, which can be used with TIDA-01518 in place of the onboard probe. Please find the links to the websites below:
Cabled probes:
https://www.cmrelectrical.com/wp-content/uploads/2013/11/RWM-Water-detection-Module.pdf
https://www.wateralert.com/wp-content/uploads/2018/08/Sensor_Cable_Inst.pdf
Also, I was able to locate an actual discrete sensor that can also be used with the TI design. Here is a link to the probe:
Sensor only:
https://www.amazon.com/Floor-Water-Sensor-Flood-Detection/dp/B079YB1T8J?th=1
I hope this gives you a starting point for the probe cables and sensors. Let me know if you need any additional information on the design. Thanks Alberto!
-Brian
Hi Brian,
thank you very much for the info!
I'll reach out if more assistance is needed.
Best regards,
Alberto