Other Parts Discussed in Thread: UCC27282, SN6501
I'm looking for a N-Channel MOSFET gate driver that can drive 2 N-Channel MOSFETs in series and allow for bi-directional current flow. See SLVA948 figure 13 for reference. All of the gate drivers I could find have reverse voltage protection which shuts the MOSFETs off in the event the output voltage is higher than the input. The input voltage is an industrial 24V so 40V is needed to allow for transients. The mosfets themselves will have a max steady state current of 15A. I'm planning on using the INA302A to regulate current and it will be DAC controlled. Any ideas on how I could drive the 2 series N-Channel MOSFETs?