Part Number: PMP7282
Other Parts Discussed in Thread: LM5116,
Dear Sir,
Is there any maximum limitation for LM5116 when going for high output current rating like 40A each phase (total 12V/80A) with very less current sense resistor value(1mE) and with the help of additional MOSFET drivers?
what is the minimum sense resistor which I can use which can be used for high current rating like 40A, that can be used for 2phase buck converter also to ensure current sharing?
thanks and Regards,
Nesh