Tool/software: WEBENCH® Design Tools
Hello everyone,
I am having some issues with the LMR36520 regarding setting Vout on Webench. It looks like whatever I add for Vin, it is only possible to set Vout between 1 and 28V. From what I've seen on its datasheet, Vout should be up to 0.95Vin. I have tried some simulations with Vin at 48V (0.95*48 = 45.6V) which is enough to have Vout above 28V.
Is this an issue with Webench or am I missing something?
Thanks a lot in advance for the support!
Best regards,