Other Parts Discussed in Thread: LM5116, OPA191
Hi sir,
Good Evening.
I am working on PMP7282, 50A, Non-isolated DC-DC synchronous buck converter and we used same schematic as PMP7282.
I have gone through following issues.
1. when we are loading at 50A Input ceramic capacitor have failed and burnt; where we are using Electrolytic capacitor (4 No, 100V/100uF. i.e. 2 for master and 2 for slave) and Ceramic capacitor (10 No, 100V/4.7uF i.e. 5 for master and 5 for slave). Please suggest us the selection criteria if we are using either only ceramic or Electrolytic or both. Which capacitor type take more voltage rating.
2. All MOSFET's have shorted at very Lower input Voltage (35V) and No-load condition, please suggest us that how to adjust the dead band time for the switching,
3. which pins have to be verified the synchronization working properly or not.
4. Both Master and slave are not sharing the load equally.
5. Please suggest, PMP7282 can be used for Automotive Application or not i.e. we want use this converter for Battery charging after rectifier output.
6. what are the possible root causes for MOSFET, Capacitor and IC failures.
Thanks & Regards,
M Khagesh