Other Parts Discussed in Thread: THS3491, THS6212, THS6222
Dear all,
I need to generate square wave signal of less than 5ns rise time and min 150mA of output current and also the inverted signal of it too. Signal generator that i am using is only capable of providing more than 5ns rise time and I tried to look for many IC's which are even capable of providing less than 2ns of rise time but they unable to produce output current of 150mA. So kindly suggest me which IC i can use with what kind a external circuitry is need to achieve my requirement.
Regards
Vinod Kanoji