This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LDC1612: Simulation, hardware & system design tools forum

Part Number: LDC1612

Tool/software: WEBENCH® Design Tools

Hello!

I'm having problems trying to import the following coil design into Eagle. It seems like the coil design tool is not compatible with the newest version of Eagle by autodesk? 

https://webench.ti.com/wb5/LDC/#/spirals?shape=Circular&lcTanKCapacitance=300&turns=18&layers=4&spaceBetweenTrace=3&traceWidth=3&copperThickness=1.500&dout=315&temperature=25&partno=LDC1612&voltage=1.8&x12=4.00&x23=4.00&x34=4.00

The Vias don't import and I played around with the DRC settings to get the TOP, INTERNAL_1, and BOTTOM error free but I can't seem to fix the Layer Setup error on INTERNAL_2. 

I'm not completely familiar with Eagle as I use Ultiboard to do PCB work so I may just be missing something or going about the process wrong.

This is what it looks like when I open the .brd file from the coil designer export. 

Any help or guidance would be much appreciated! Thanks!