This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00630: can TIDA-00630's mini displayport can reach 4K(3840x2160) up to 60HZ?

Part Number: TIDA-00630

Hi Team,

I am going to built-in a type-c dock in one of my product. Looks like that TIDA-00630 is a good choice. There are some unclear that i would like to ask:


1. Can it reach 4K at 60HZ when it connected to a Mini Displayport monitor?

2. How much bandwitdh can the USB downstream port can have when it's running a 4K@60HZ monitor?

Thanks.