Part Number: PMP4484
Hi,
What is the part number of the transformer? I'd like to order some and build PMP4484 to test out the application.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi the transformer for PMP4484 is from GCI Technologies, the part number is G095024LF
You can contact Saul Landros for more information
Saul Landeros <saul.landeros@gcitechnologies.com>
Thanks,
Robert
Hi Robert,
Thanks for the update.
I was looking into the datasheet of G095024LF provided by GCI, but the footprint and the inductance value of the transformer don't seem to match the info on PMP4484.
G095024LF (provided by GCI): 100uH, size 31.5mm x 31.5mm
EDR3909, PC95 (found that part from another TI Forum thread): 475uH, 15mm x 55mm
Can you please help verify the transformer T1 info?
Thanks,
TI- Forum PMP4484 Transformer.pdf
Thanks,
Hi Harry,
So sorry for the trouble here, I mistyped the design number, so that transformer from GCI is actually for PMP4844, not PMP4484 that you asked about.
The correct part is the one that you referenced from the previous thread. Again, sorry for my mistake.
Thanks,
Robert
Hi Robert,
Thanks for the clarification. Unfortunately, I wasn't able to find/order the EDR3909, PC95 anywhere in the market. Any thought where I might be able to find and order them? If not, do you have any alternative part for that transformer?
Thanks,