Tool/software: WEBENCH® Design Tools
Hi,
I am using CSD18510Q5b mosfet .RθJA of Mosfet is 125°C/W with minimum pad area.Now if i used copper 10mmx10mm copper pad with 2oz copper thickness then approximate θCu=35°C/W.So can i use RθJA and θCu in parallel to reduce total thermal resistance.(125°C/W || 35°C/W = 28°C/W ).