Part Number: TIDA-00792
Other Parts Discussed in Thread: CSD13381F4
Hello TI experts,
I am considering TIDA-00792 for designing BMS for my device with following configurations.
Number of cells in series: 12
Cell max voltage : 4.2V
Battery max voltage : 50.4V
I have confusion regarding external FET circuit. The external FET is fed voltage through 10K ohm resistor. My question is, how much gate of FET need minimum current to turn ON or pull in saturation region.
I have calculated current with my application. When voltage across cell is 4.2 V then maximum current of about 0.21 mA can pass through 10 K ohm resistor. Is this calculation correct? Is it enough to put FET in saturation region? I know that FET is voltage controlled device but 0.21 mA is very less according to me. Kindly explain it
Thanks
Best regards
Imran Riaz