Part Number: TIDA-00817
Other Parts Discussed in Thread: BQ76PL455A-Q1, EM1402EVM
Hello.
This is the following thread of "https://e2e.ti.com/support/tools/sim-hw-system-design/f/234/t/883441"
I successfully connect between TMS570 and My host PC with bq76PL455_GUI by opening COM port.
I have a problem while operating gui with balancing On button.
As a result, Balancing is not working.
With the 16 batteries, I put 13 batteries as a normal cell which has 3.7V and 3 batteries as low SOC cell which has 3.5V
I click the Balance-on button at 25 sec. here is the result screenshot of normal cells.
here is the result screenshot of Low SOC cells.
Compare with the result from TIDUBI0, p16, P17, It is definitely wrong.
For the solution, I checked the connection again. Cause I think the signal from the MCU is wrong first.
Here is the question.
Which connection guideline should I follow for the "http://www.ti.com/lit/zip/tidcbz0"
or