Part Number: PMP40379
Other Parts Discussed in Thread: PMP, , UCC256402, UCC256302, UCC256404
Hello,
I am developing this system for audio power system supply using the PMP
40379.
I am testing only for 115VAC.
QUESTION
1. Is S600 short for 115VAC connect from COMPONENT GBU8J-BP pin 2 & L601 pin 3 To =>> C605 negative rail?
~115VAC SHORT: Is this the optimal connection for 115VAC without the Switch? This is for USA market!
2. For the DNP R613 , if I don't populate this resistor i.e. R613, I would still have to make the connection for SS from PIN 9: LL/SS to PIN 12: RVCC correct?
Also can I use a 0R instead of
Just need some clarification, thank you.
Regards,
Neil Henry
IRADLLC