Part Number: TIDA-01243
Hi TI team
we planing to design-in your USB-C to HDMI+ Charging solution into our main PCB, I just order TIDA-01243 EVM and received today, I'm facing some issue during test.
1. When I try to mirroring android phone or Samsung Dex to LCD monitor via HDMI, the screen looks unstable and blinking few times. got HDMI CONNECT/DISCONNECT ...
2. When I connect 5v/1.5A power source into J30 charging port got nothing , that means no charging current flow to the phone.
3. Is the barrel jack input only accept 20v input ? can pump in DC_5v to start the EVM working and charging phone or not?
Do I need any setting or upgrade firmware before use the EVM and how to setting ? appreciate if able to get your fully support to speedup our product,
Thanks
RUI