Part Number: BQ40Z50
Other Parts Discussed in Thread: BQSTUDIO
Tool/software: WEBENCH® Design Tools
Dear TI members,
Good day.
I used BQ40z50 IC. (Default srec is bq40z50R3_v3_09_build_73)
When we make a pack, and we're running a Charging and discharging test, However, the Remtimealarm changes from 10 to 375. (Setting value : 10)
And the cycle count soon changes to 65535.
However, if We see Log status at this time, an error seems to occur.
So, I wonder. As above, the reason why RemtimeAlarm changes and the reason why Cycle count changes.
Is it a communication error or a problem setting the GG file? When an communication error occurs, are these values likely to change suddenly?
Please check.
Thanks.