This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMZM33602: Integration of different TI modules

Part Number: LMZM33602
Other Parts Discussed in Thread: TPS63021, LMZ34002

Tool/software: WEBENCH® Design Tools

First, I want to do simulation of LMZM33602,LMZ34002 and TPS63021 power modules and converters in other than WEBENCH design tools if possible. Second i want to make combined schematic of these modules in altium designer (then layout) . I was not abled to integrate WEBENCH altium connector in Altium connector perhaps due to my cracked version of AD. Please guide me in this regard which way i should proceed.

  • Hi Ahsan Ameen,

    You can download the spice models from ti.com and import them into any of your favorite CAD tools. For example for LMZM33602, the product folder (https://www.ti.com/product/LMZM33602/toolssoftware) has un-encrypted PSPICE model which should work in any PSPICE compatible tool.  The product folder also has an encrypted model, which is validated in Cadence Allegro (OrCAD) . 

    You can also integrate multiple schematics in simulation tool of your choice. If you face any issue with  the 3rd party tools - please  direct your questions to the respective tool provider. If the issue is with the spice model - please post your issue to the respective product support forum and product experts can help you further. 

    Regards,

    Srikanth Pam

  • Thanks Srikanth.. i saw it earlier but i was bit confused with transient word.Ok I see it. I also want to import them (all schematic together) in PCB layout software like altium designer. For that what you suggest.Thanks