Part Number: PMP10725
Other Parts Discussed in Thread: LM3481
Hi,
We need 5 isolated output as below,
| Output Voltage 1 | 24VDC/200mA |
| Output Voltage 2 | 24VDC/150mA |
| Output Voltage 3 | 24VDC/160mA |
| Output Voltage 4 | 24VDC/250mA |
| Output Voltage 5 | 24VDC/140mA |
In PMP10725, there are 3 isolated output(24V, 16V and 16V)
Our input voltage:24VDC.
Can I use this reference design if I change transformer with 5 outputs.
Will it work?
Guide me with some suggestions.