This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP7760: Stability Calculation

Part Number: PMP7760


Hello,

At the PMP7760 how do i calculate the Stability Loop Componenets? (R107,C106,C107)

Thank you

  • Hi Maor,

    Please refer to the current mode control flyback topology section and type-II compensation network equations in this pdf: 

    https://www.ti.com/seclit/ml/slup340/slup340.pdf

    In short, what you should do is:

    1) Determine the power-stage transfer function of the flyback converter (look for the right-half plane zero frequency)

    2) Select your cross over frequency and phase margin, with respect to the right-half plane zero

    3) Since you are using a type-II error amplifier, you should make sure that your zero of the error amplifier is a decade (1/10) of your crossover frequency, and high-frequency pole is at your right half plane zero.

    Thanks,

    Richard