Part Number: TPS61175-Q1
Other Parts Discussed in Thread: TINA-TI, LM5022
Tool/software: WEBENCH® Design Tools
Hi,
I try to add TPS61175-Q1 TINA-TI Average Spice Model in TINA-TI.
I copied the TLD, LIB, TSM files into "c:\Program Files (x86)\DesignSoft\Tina 9 - TI\SPICELIB\" folder.
Then I restarted the tool, and said Yes to rebuild the library.
But I see the endless question:
"The selected micro is not present in the library index.
The library needs to be rebuilt.
Re-build the library?"
Then I tried commands: Tools - Re-read symbol database, Tools - Re-compile library, Tools - Re-build library.
No effect.
I can use the model only using the "Insert - Macro..." command.
I also tried to use the LM5022 TINA-TI model. The same result.
How to add models to the TINA-TI internal library?