Other Parts Discussed in Thread: LM5022
Hello,
I have some questions regarding the PMP7760 development circuit:
1) How do i choose the maximum duty cycle? the maximum duty cycle of LM5022 is 0.90, can i choose for the minimum input voltage (lets say 12V in my design) duty cycle of 0.89? or there is an equistion to calcultae the maximum duty cycle? what will be than the minimum duty cycle at the maximum input voltage?
2) How do i calculate the secondary widing turns? can i use the formula (Vo+Vdiode)*Np/Vinmin ?
3) The design is CCM or DCM?
4) How do i calculate R106 if i want minimum input voltage of 12V?
Thank you!