Part Number: PMP7760
Other Parts Discussed in Thread: PMP20745
Hello,
At the PMP7760 Design, Can i work with DCM mode?
My design have 12-700VDC input voltage and output current of 1A and 9W
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PMP7760
Other Parts Discussed in Thread: PMP20745
Hello,
At the PMP7760 Design, Can i work with DCM mode?
My design have 12-700VDC input voltage and output current of 1A and 9W
Thank you
Hello Maor,
PMP7760 operated in DCM at lower load current and higher input voltage..
It operates in CCM at higher load current and lower input voltage.
You will exceed the maximum duty cycle operation at 12V input with this design. In this case you will need to redesign the power stage, basically transformer turns ratios, then review power component stress and losses
Please compare PMP7760 to PMP20745 to get an idea of control circuit changes.
Best Regards,
Bob Sheehan
Power Design Services