Part Number: TIDA-01168
Other Parts Discussed in Thread: LM5170, LM5060-Q1, LM5060, LM5170-Q1, TIDA-01167
Hello.
Please tell me about TIDA-01168.
Q1: JAU275B Page55 has the following description.
>The jitter size is ±3 × tADC_chan_sampl, where tADC_chan_sampl is the channel sampling period.
>The jitter size should not exceed one-tenth of the control loop cycle tctrl_loop.
Why shouldn't it exceed 1/10? What happens if I exceed it?
Q2: Figure 14. In the schematic of the 48 V circuit breaker, the overcurrent threshold is determined by R103: 2.87k and R104: 20.5k, but the current direction in which the overcurrent protection function works is KL40-> P48V . (BUCK operation) only. It does not work with P48V-> KL40 (BOOST operation).
Is my understanding correct?
Q3: Figure 20. 12V circuit breaker schematic, 12V reverse connection protection is not possible even when MOSFET is off. Additional circuitry with PMOS and diode is required separately as described in LM5170 E2E.
Also, to turn off the 12V circuit breaker, it is necessary to drop pin27 (FAULT) of the LM5170 to LOW, so this converter circuit cannot be turned off.
Is my understanding correct?
Best regards,