Part Number: TIDA-00527
Other Parts Discussed in Thread: THVD2450,
Hi,
Correspondence with TI is given below. Do you have any comments?
Thanks...
******************
Dear Ahmet,
I have reviewed the attached file, unfortunately, our support is limited to only TI's published resources and documents. At the moment, the resources we have are limited to address all your inquiries. This will still need the expertise of our application engineers. Kindly consult them instead by posting the inquiries at the E2E: https://e2e.ti.com/p/addpost?fn=138
Let me know if you need assistance with the E2E or if you'd like me to post it on your behalf.
Regards,
Elisha Tarroza
Texas Instruments Customer Support
************************************************************************************************
Hi Elisha,
Thank you for your quick reply.
In the question / answer section you submitted; If the cable used is short and the speed is low, it seems the problem is. For 24VDC BUS transmission, THVD2450 seems to be available. In this type of bus transmission, it appears that there is no constant voltage level. Also; You have indicated that the values of Inductor, AC coupling capacitor, termination resistors, pull-up and pull-down resistors on lines A and B are important parameters.
I will have a few questions to clarify the issue;
1) We want to use an RS-485 power over bus of about 1Mbps over approximately 24VDC. How fast can we transfer data at a distance between 100m-200m?
2) Approximately 16 sensors (node, point) will be used on the bus. In total; A current between 200mA and 250mA for 16 nodes will be transmitted on the main bus line. Cable lengths from all nodes are approximately within the range of 100-200m.
In this case, how much current and dc voltage transmission can be achieved? Considering that CAT6 cable is used; voltage drop will be a nuisance for 200m cable. In this case, it will be necessary to use thicker cable. Or what is your suggestion?
3) You suggest regarding data rates and cable lengths; I have previously reviewed the document “www.ti.com/.../slla431.pdf”.
References:
Best regards......
Ahmet Turan ALGIN
************************************************************************************************
Hi Ahmet,
Thanks again for contacting TI.
This is your case through which we will continue to communicate with you. You may reply either through your myTI portal or through the email that you will receive.
Please give me 24~48 hours to get back to you for any update.
Regards,
Elisha Tarroza
Texas Instruments Customer Support
************************************************************************************************
Hi...
I want to use the TIDA-00527 demo board. I want to make RS485 communication in a wind turbine with power over bus. In this case; How far can I transmit with this circuit?Secondly, how long will the transmission speed be for 100-200m? Third, 3.3VDC is used here. If 24VDC is used, how is the situation?
Best regards......
Ahmet Turan ALGIN