Part Number: TIDA-01606
How easy would it be to modify it to operate at 125V DC input and 10KW ? What changes would be required ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01606
How easy would it be to modify it to operate at 125V DC input and 10KW ? What changes would be required ?
For this design to operate at 125VDC at 10kW power will require a complete redesign of this board. Currently this design can handle a max of 18A, for this to be designed tor 125VDC operation, we are looking at redesigning this board to handle (Power/Voltage = Current i.e. 10,000/125 = 80A plus 20% margin) ~100A of current. That will require a complete redesign of switches (SiC & IGBT) and magnetic components along with board layout redesign to handle this current.
TIDA-01606 is a three level T-type inverter topology targeted towards being able to address 1000VDC or higher using lower V rated switches (SiC & IGBTs) in multiple levels. This topology is not well suited for a 125VDC design. Hope this helps.
Assuming this is 125V variable voltage input coming from a Solar string array, I would suggest looking at TIDM-SOLAR-DCDC in tandem with TIDM-SOLAR-ONEPHINV to address this power conversion.
TIDA-01606 is not the best topology/ design to address 125V from a solar string array.