Part Number: TIDA-00721
Hi team,
Where is the software of TIDA-00721?
How can I apply for the EVM of TIDA-00721 and NFC-READER?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-00721
Hi team,
Where is the software of TIDA-00721?
How can I apply for the EVM of TIDA-00721 and NFC-READER?
Thanks!
Dear Naizeng -
the firmware is attached here: TIDA-00721_Firmware_v1.0.zip
Dear Naizeng -
As it states on the TIDA-00721 page, under the image of the patch, next to the description of the design -
Fully assembled board (shown above) developed for testing and performance validation only, not available for sale.
The design files are provided for your reference and if desired, to order from a board assembly house of your choice.
The reader is an NFC enabled handset (phone) or tablet (most Android models, perhaps the other OS based one now, too) or can be made from:
http://www.ti.com/tool/CC3200_NFC_CARD_READER
or
Dear Naizeng -
if you mean for the reader, from TI, then this soft bundle link which is found via one link I provided earlier will suffice.
https://www.ti.com/store/ti/en/cart
this will give you MCU and NFC/RFID platform with which to activate the tag/transponder w/temp sensor, that you will have made from the reference design files.
i did just notice that the NFC/RFID BoosterPack is out of stock on our store, these can be had from here, they have 97 in stock
Hi Josh,
Thanks for your support!
I mean how to apply for the fully assembled board of TIDA-00721?
Naizeng -
The design files are available for you to have made. We do not have these available to send out. This is the purpose of the wording on the product page of the reference design.