This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS54202: operating conditions updates revert components to default value

Part Number: TPS54202


Tool/software: WEBENCH® Design Tools

If we create custom parts and then update any of the operating conditions (temperature, voltage, or current) the component values revert to its default value. As an example, I used the TPS54202, changed the output capacitance to 100uF. After I modified the maximum operating temperature to 85°C, the capacitor value switched back to 22uF. The issue does not occur if I reverse the order of this exercise by changing the operating conditions first. This becomes a nuisance when experimenting with operating conditions and few of the components are deviated from their default values.

Can you please comment whether this is something that can be fixed?

Thank you!