Part Number: PMP6712
Hello.
I want to refer to your PMP6712 case to design a 48V input, 50V / 20A / 1000W single DCDC power supply.
I initially learned the schematic diagram of PMP6712.
I have some questions to ask.
1. Is this reference case working simultaneously? Does each channel output 800W of power?
2. I only need to do a single-channel 1000W case. For the first and second sheets in the schematic, can I refer to one?
3. The first and second sheets of the schematic diagram should be the main power, controller, and driver parts. I don't understand what is the function of the SUNB circuit composed of 6 diodes?
4. I only do the single-channel DCDC main function, the third schematic, do I only need to refer to the bias power supply and op amp feedback section? No over-voltage protection and active buck snubber circuit are required. I don't know what is the function of this active buck snubber circuit?
Thank you.