Part Number: PMP6712
Other Parts Discussed in Thread: UCC28950, UCC28951
Hello.
I need to design a DC / DC power supply with a rated 48V, an input voltage of 38V ~ 58V, and an output of 50V / 20A / 1000W.
I want to refer to the PMP6712 design case you provided. In this case, the DC / DC power supply specifications are 38V ~ 60V, and the output is 54V / 15A / 810W.
Your reference cases have helped me a lot.
Due to the urgency of the boss in this case, I have not done a similar circuit before, and it takes a certain time to learn to digest and then make a prototype. I wonder if I can ask for more help:
1. Whether a 50V / 20A / 1000W development board can be customized, the cost can be negotiated.
2. How can I buy the PMP6712 development board if it cannot be customized?
3. If the PMP6712 development board cannot be purchased, I change the design by myself. What parameters do I need to change?
4. Can you provide a more detailed calculation design book and simulation model for the design case? I found other calculation and simulation cases based on UCC28950 on the official website, but no PMP6712 calculation and simulation data.
The PMP6712 design case you provided has helped me a lot, but the development time of this case is too urgent. If you can give more support, it will better promote the development and production of this product.
Thank you!