Part Number: TIDA-010054
Hello
I am going to design bidirectional DC/DC conveter. Here are the design parameters. Uin=400V, Uout=from 44V to 58V, Pout=3000W. Which type of converter is better solution Dual active bridge or CLLLC?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-010054
Hello
I am going to design bidirectional DC/DC conveter. Here are the design parameters. Uin=400V, Uout=from 44V to 58V, Pout=3000W. Which type of converter is better solution Dual active bridge or CLLLC?
Thank you
Hi Martin,
Thank you for the query.
Given your requirement of fixed bus voltage of 400V and variable battery voltage, Dual Active Bridge is better than a CLLLC. But it will come at a cost. A large variation in phase will be needed to regulate the output voltage and it can increase circulating currents and can hamper efficiency of converter. This where Dual and triple phase shift schemes for DAB can be helpful in increasing the efficiency marginally.
If there is room for you to vary the bus voltage by 10%, I think CLLLC will be better than DAB. In the CLLLC, in addition to the normal resonant modes of operation additional phase shift can be used as a control parameter to improve operating range.
Thank you
Regards
Hello
I have already simulated both of the types converter. Switching frequency was 200Khz for both converter. In CLLLC converter secondary LR2 is too small 250nH because it depends on resonant frequency,turns ratio and output power. I am afraid of it becuase so small inductance can be in secondary leakage of transformer and it can be difficult to abide in serious production. Please what do you think about this problem?