Part Number: OPA1678
Other Parts Discussed in Thread: OPA1612-Q1
Tool/software: WEBENCH® Design Tools
Hi Sir,
The attachment is the BPF+OPAMP's schematic for TINA. In real board when switch on, we can measure the voltage of VF2 about 4V VPP, but after 1 day, the voltage will become 3V VPP.
We found that VF1&VF2 output voltage decrease with time. What is the problem for schematic?
Meanwhile, my application is that when using a variable resistor(R18) to adjust the required VF3 voltage. I hope the voltage drifts within 1V on VF3 and 0.2V on VF2.
Regards,
Roger