This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools: Current through inductor AC analysis

Tool/software: WEBENCH® Design Tools

Hello,

I'm trying to simulate the frequency response of current through inductor. Circuit is as shown below, where VG1 is voltage generator (sine wave 10V, 50Hz), Inductor and resistor.

My question is, if i'm doing AC analysis, is the amplitude waveform generated is the result of Iout/Iin? Because from the results you can see that as the frequency increase above 1Mhz, the current through

the inductor start to roll off. But in here there is no Iin included because there is no current source, just voltage generator as the input and IL is the output. How does TINA compute the AC analysis? Thanks