This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tina TI Import TVS Netlist

Hello,

i trying to import the following netlist into TinaTi:

.SUBCKT 5.0SMDJ26A 1 2

* TERMINALS: A K
Done 1 2 Dtvs
Rleak 1 2 52meg
.MODEL Dtvs D (IS=1.0e-5 RS=0.0902 N=1.5 IBV=1m BV=30.40 CJO=6700p)
.ENDS

If i compile this netlist in the Netlist Editor, i get the following error message: "Invalid .ENDS command. Line 6"

, without the .ENDS command the netlist is compiled successfull. But when i tried to import this modified netlist with the "New Macro Wizard" i got the following message: "This circuit cannot be converted into a macro"