Part Number: LMR33630
Tool/software: WEBENCH® Design Tools
Hi team,
My customer considers to use LMR33630BDDA and he is using Webench for the design.
When he set Vinmin=Vinmax=12V, Vout=8V, Iout=0.3A, Temp=30℃ then design can not be created as attached.
In case of other load current like 0.2A, 1A etc, design can be created successfully.
Also, in case of other package (WSON), there is no problem even if it's same input voltage, output voltage, output current.
Is this just due to error of Webench?
Best regards,