This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01623: TIDA-01623

Part Number: TIDA-01623


Hello,

We are looking for a concept for the design of a PS used for a display supply, 5V, 16A, 80W with the following voltage range input: nominal input 110V DC +-30% = 77-143VDC. Ambient temperature is up to 80°C.

The concept used in the DesignGuide:TIDA-0162330-W/in3, 93.4%Efficiency,100-WAC/DCAdapterReferenceDesign seems to be suitable.

Can such a concept run with a DC input votage of 77V?

Best Regards

Peter Michel

peter.michel@terepco.eu