Part Number: TIDA-01418
Hi,
My understanding of programming the microcontroller (which is controlling an inverter) is first to power off the high voltage DC bus, then to program the mictrocontroller. This is because the states of the peripherals are not determined during the programming process, and there is a chance that a shoot through can happen, unless there is external circuits to prevent this from happening.
For TIDA-01418, to re-program the MCU, we should turn off the 400V DC bus first, then program the MCU.
Is this correct?
Thanks.