This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM73606: ripple calculation

Part Number: LM73606

Tool/software: WEBENCH® Design Tools

Hi Champs,

could you please help me answering the following questions from a customer:

Vin min. 19V and Vout 16V @ FRQ 400kHz?

1)
If we change "Max Vout Ripple" under Configuration Options, nothing changes regarding the Vout Ripple in the design with the Cs and in the Operating Values ​​Categorie / Systeminformation listing.

2)
If we change the value under "max Peak to Peak Inductor Ripple" in%, the L value in the design does not change, nor does the value in the Operating Values ​​Categorie / inductor

3)
If we change "Mode of BIAS Operation" from e.g. VOUT to GND,
the IC Power dissipation and Tjunction in the Operating Values ​​Category / IC does not change.

Are these still errors in the designer, or is there a user error by us?

After these changes show no reaction in the design or the category list, I would like to ask if the phase margin values
be calculated correctly.

Thanks a lot in advance.