This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00779: R38, R27, Current Limit Resistor Bypass Circuit

Part Number: TIDA-00779


hi 

i have a question.

There are two things I don't understand about Current Limit Circuit.
Q1) Are the device values of R38 (21k Ohm) and R27 (221k Ohm) correct?
R38(221k Ohm) and R27(21k Ohm) Isn't that what you should do???

Q2) I can't understand Switch On delay 0.2s.
In other words, I don't understand the circuit. Please help.

  • Hi jaeyup,

    Q1: The value of R38 is ok.

    Q2: Regarding the 0.2s delay, it is obtained by RC delay, simply you can observe the base voltage of Q5 using oscilloscope while PFC_ON no connected, the base voltage should rise to the ON thresh voltage of Q5 after power on 0.2s. Of course, this delay time should be related with input power voltage, we do not need to control a very precise time here, if your system has a MCU, you also can control the relay by MCU IO pin directly.

    Felix