Part Number: BQ24650EVM-639
Other Parts Discussed in Thread: BQ24650
Tool/software: WEBENCH® Design Tools
I have a question during the bq24650evm-639 exam.
1. The datasheet says that if the mppset pin voltage is below 1.2v, the charging current decreases to maintain the charging state.
2. The mppset power of bq24650evm is 17.8V.
3. We change the input voltage with the power supply and proceed with the charging test.
4. When the input voltage becomes 17.8V or less, the mppset voltage becomes 1.2V or less, so the charging current must be reduced, but the charging is cut off and then charged again when the input voltage is raised to 17.8V or more.
Questions
-Please tell me how to keep the charging state by decreasing the charging current when the mppset voltage falls below 1.2V
DASHEET(BQ24650)
8.3.2 Input Voltage Regulation A solar panel has a unique point on the V-I or V-P curve, called the Maximum Power Point (MPP), at which the entire photovoltaic (PV) system operates with maximum efficiency and produces its maximum output power. The constant voltage algorithm is the simplest Maximum Power Point Tracking (MPPT) method. The BQ24650 automatically reduces charge current so the maximum power point is maintained for maximum efficiency. If the solar panel or other input source cannot provide the total power of the system and BQ24650 charger, the input voltage drops. When the voltage sensed on the MPPSET pin drops below 1.2 V, the charger maintains the input voltage by reducing the charge current. If the MPPSET pin voltage is forced below 1.2 V, the BQ24650 stays in the input voltage regulation loop while the output current is zero. The STAT1 pin is LOW and STAT2 pin is HIGH.