Part Number: TIDA-01426
Other Parts Discussed in Thread: TL494
Hi TI experts,
My customer reviewed TIDA-01426. they want to design output 300V, max 0.5A. (input 12V)
Is 150W design possible with flyback block using TL494?
If it possible, please guide the circuit that needs to be changed.
If not possible, Please provide a solution that can design specs below.
Input : 12V
output : 300V, 0.5A or 0.3A
Thanks,
Downey Kim