Other Parts Discussed in Thread: FDC1004
Tool/software: WEBENCH® Design Tools
Hello Dear TI team support
I need to implement in my devise a TOUCH sensor.

should be maximum of 50 cm from main board.
Touch sensor requirements
The Touch sensor is connected to a “metal gate” using a metal screw (See picture TOUCH_1.jpg). When the rodent enters the bait station, he touches the “U” shape “metal gate” (see the 40 mm strip at the button of “metal gate” as seen in picture TOUCH_2.jpg) and triggers the touch sensor.
Please help me understand how can I create it, please suggest components and connection.
Best regards
Ilya