Part Number: TIDA-01606
Other Parts Discussed in Thread: TMS320F28379D, , SFRA, TMS320F28335
Tool/software: Code Composer Studio
Dear Sir,
Just now I got my new control card and docking station for TMS320F28379D. I have ported a code for TIDA-01606 on this board and also connected analog signals
to ADC pins as shown in documents. I can control I/O on the board by toggling the LEDs .Also I have checked Relay ports as configured in TIDA-01606.
My problem is
1. I cant see the proper RMS values for Voltage and current and also other power parameters.I have observed 50 Khz frequency for sampling for the the function read
2. PC not able to detect USB port when connected UART terminal.(Both switches in ON position).
3.Please guide me how to use SFRA GUI to see the parameters
Presently I am using TMS320f28335 and able to read analog signals and done D-Q transformations ,SPL and generated PWM signals as per input.
Also ,can you suggest what documents I should refer to understand the software flow of TIDA-01606
Regards
Manish