This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TMDSRM48HDK: Simulation, hardware & system design tools forum

Part Number: TMDSRM48HDK


Tool/software: WEBENCH® Design Tools

The pins numbers of the headers: J9,J10 (66 pins) and J11 (80 pins) are labled a strange/unlogical pin sequence. 

Shouldn't they be labeled with the pattern 1 2..........65 66   instead of 1  2 ......... 66 65 (as it is printed)

How should I read those pins numbers? Thanks