Part Number: TIDA-01606
Other Parts Discussed in Thread: SFRA
Dear Sir,
Started working with F28335 and after implementing ADC, PWM, D-Q conversions ,Power analyzer and SPLL now shifted to F28379D . As TDA-01606
is a reference design near to my final product.Got my docking station and control card of F28379 D . Ported TIDA-01606 code and observed I/O operations and ADC
sampling. Sampling is done at 50 Kz .Now I need help on following points:
1) It was observed that all the RMS values showing zero though accumulation of sum is there. After doing few modifications in the code now I an see RMS values and other
power parameters in the structure .Please tell me what will be the cause also is there any GUI where I can see all these parameters?
2. After connecting USB port to PC, the is showing " newly connected port malfunction " but if I download SCI example code it works Fine. Switch position is in "ON"
3. No PWM pulses are observed on PWM output though there is grid voltage ,current present.