Part Number: PMP4497
Other Parts Discussed in Thread: TPS53632,
This design has the output voltage max at 1.2V, do you have any designs that go from 48V to 1.8V?
It looks like the TPS53632 limits the voltage to 1.2V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Juliana,
at "standard" controllers min Vin is limited to Vref due to virtual short circuit at OpAmp input;
this device got some more IP in it. Despite Vref 1.7V the 6-bit VID i/f allows Vout 500mV to 1.52V
by resolution in 64 steps.
BUT: another limitation needs to be considered by input voltage, switching frequency and number
of phases - i.e. at Fsw 1MHz max. output voltage is 1.28V !
The spreadsheet helps to figure out the suited Fsw according to needed Vout.
Best regards, Bernd