Part Number: TIDA-00002
Other Parts Discussed in Thread: SFRA, , C2000WARE, POWERSUITE
Hello,
I am currently testing the TIDA-02002 and referring the design guide Rev C. As per the design guide section 3.2.2.4.1, the instruction says select "Lab 3: Closed Loop:Current" under project options and select current loop under SFRA option. And after saving this, the Comp Number and Comp Style will automatically selected as 2 and DF22 respectively. But when I follow the above instructions, the Comp Number I am getting is 1.Can you help me understand why?
Another thing since I need to run lab 4, I should select Lab 4 under project options right? When I select Lab 4 and launch the Compensation Designer tool and select the SFRA data for current sweep from lab 1, the Comp type and the Coefficients do not match. Even the Loop at the bottom says Unstable Loop.
Can you please help me run the Closed Current loop lab for this design?
Thanks,
Abhishek