Part Number: LM2698
Other Parts Discussed in Thread: TPS61099, TPS61089
Tool/software: WEBENCH® Design Tools
Hello,
I have designed a 6.5V boost circuit by Webench tool.
Attached is the design report
Can you check the report and can we expect the efficiency mentioned by Webench design?
I have the following constraints:
Vin minimum: 3.0V , Vin maximum: 3.67V
Vout: 6.5V, Iout maximum: 50mA
Maximum allowable height is 2mm. Only 1 component can be above 2mm but that too should be below 2.8mm.
Only shielded inductors
Only ceramic caps X7R, C0G/NP0, X5R ..... X5R to be used as last resort.